AXIS#.SAFEPARAM.SLS_#.FAULTREACTION

Description

Indicates the safety function activated when Safely Limited Speed (SLS) is faulted. One of the following values can be used:

Value Description

1

STO

2

SS1 Instance 1

3

SS2 Instance 1

 

Parameters Editor with the Fault Reaction options showing and circled

Context

For complete SLS information refer to SLS (Safely Limited Speed).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

1, 2, 3

Default Value

1 (STO)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLS_1.FAULTREACTION

315ch

0ah

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_2.FAULTREACTION

315dh

0ah

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_3.FAULTREACTION

315eh

0ah

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_1.FAULTREACTION

325ch

0ah

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_2.FAULTREACTION

325dh

0ah

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_3.FAULTREACTION

325eh

0ah

Unsigned8

-

-

Read/Write

No